You are here: Using KAS Simulator > Custom IO Editor Tab

Custom IO Editor

Each I/O is displayed based on a tree-structure representation. The structure is the counterpart of the formatting used in the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger to define I/Os address within the I/O editor (see Modify Input/Output).

I/Os Displayed in Object Tree

Figure 6-6: I/Os Displayed in Object Tree

I/O value can be displayed according the following formats:

I/Os Value

Figure 6-7: I/Os Value

See also Custom Input/Output Editor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™